This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3DV642-Q1: Need Simillar Mux

Part Number: TS3DV642-Q1

Hi Team,

Please provide the 1:2 mux for CSI2 Application which supports speed Up to 5.7 Gbps per trio.

  • Hello Thrinesh,

    The TS3DV642 can pass 6Gbps on each channel and has 2:1 configuration. 
    It should be able to support CSI2 applications if the signals you are trying to pass through it fall within its recommended operating conditions.

    What about this device doesn't meet your needs?

    Thanks,

    Nir