Part Number: TUSB8020B
Other Parts Discussed in Thread: TPS2561A,
Hello,
I have boards manufactured and I'm trying to debug the USB interface. The issue I'm seeing is the TPS2561A is not getting the enable signal from the TUSB8020B. I don't know if the Hub is in a sleep state or if I incorrectly configured the standalone mode.
I have verified I am getting all of the correct voltages at the VDD and VDD33 pins.
I do see voltage at XI from my external oscillator.
Pins 2 and 3 (SCL and SDA) I had them floating, but I also tried pulling down to ground
Pin 22 (SMBusZ) I had pulled down to ground and I tried it floating
Pin 9 (Usb VBUS) I'm getting around .5V
Pin 11 (GRST_In) I'm getting around 3.2V
I'm not sure what else to check or what would be causing the TUSB8020B Not to send the enable signals to turn power to my downstream devices.
Thanks
David