Part Number: TS3DV642-Q1
Hi Team,
Can you provide CPHY CSI2 supported speed per trio for the part TS3DV642-Q1.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TS3DV642-Q1
Hi Team,
Can you provide CPHY CSI2 supported speed per trio for the part TS3DV642-Q1.
Hello Thrinesh,
At what specific signal speeds are you planning to operate at?
The TS3DV642-Q1 is a passive mux, so it can support passing any signal as long as its voltage level and speed are within its specifications.
Thanks,
Nir
Hello Thrinesh,
Understood, thank you for clarifying.
Unfortunately, we don't have a device specked for 22.8Gbps.
The closest one is the TMUXHS4412, which is specked up to 20Gbps.
Though, its bandwidth is 13GHz so it might be able to support your speed requirement.
You can order some samples with an EVM to verify.
This is the best solution we currently have for this.
Thanks,
Nir