Part Number: TUSB7320
Other Parts Discussed in Thread: TUSB7340, TUSB7340-EVM
Hello,
I am testing a design which uses the TUSB7320IRKM, and it is behaving unexpectedly.
When a USB 2.0 device is connected, the enumeration process fails. Windows 11 device manager indicates that a USB device is connected, but is not functioning correctly (device descriptor request failed).
The USB high-speed detection handshake process appears to begin normally (see fist attached image), but the K-J chirping does not cease before the 10ms reset period is exceeded, and the process restarts after ~100ms (see second attached image).
I believe this to be caused by a hardware configuration problem, however, I have been unable to identify the cause of the issue.
What is the recommendation for next troubleshooting steps?
Additional details:
This TUSB7320 implementation is question is based on the TUSB73x0 datasheet (Rev Q) and TUSB7340EVM reference implementation (with preference to the datasheet for differing parameters), but without an attached EEPROM and with only the USB 2.0 signals connected. All USB 3.0 pairs are not connected in this design. The TUSB7320 initializes successfully as a PCIe endpoint, and is recognized under Windows 11 with the SLLC448 version 01.00.00.0A driver.
Attached figures:


Note: Oscilloscope measurements are taken using a differential probe.