Part Number: TCA9509
I would like to confirm whether it is acceptable for Port A of the TCA9509 to be pulled up by a connected device.
- Device: TCA9509
- The datasheet states that a pull-up resistor should not be connected to Port A.
- In my system, the device connected to Port A (a sensor) has a pull-up resistor on the line.
Because of the sensor configuration, Port A is effectively pulled up through the connected device.
- Is this configuration acceptable, or could it cause any functional issues with the TCA9509?
- If this configuration is not recommended, what failure mode or risk should be expected?