This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1043A-Q1: Power Dissipation Calculation

Part Number: TCAN1043A-Q1

Hi Team,

I am trying to estimate the power dissipation of the TCAN1043A-Q1 CAN transceiver.

From the datasheet, I considered the device power dissipation as:

PD=VCC×ICC

For my case:

  • VCC=5V
  • ICC=70mA

So the calculated power dissipation is:

PD=5×0.07=0.35W

My understanding is that this 350 mW corresponds to the IC power dissipation used for thermal calculations.

Could you please confirm if this approach is correct for TCAN1043A-Q1, or if additional contributions such as VSUP current and CAN bus driver losses should also be included?

Thanks.