This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TC811-Q1: Link Failure

Part Number: DP83TC811-Q1
Other Parts Discussed in Thread: USB-2-MDIO, DP83TC811EVM, DP83TC811

Hello,

This is a question from a customer in charge. They are evaluating the IC with the following configuration.

PC ― DP83TC811EVM ― DP83TC811EVM ― PC,  using USB-2-MDIO

Symptoms include:

If the PC is set to 100Mbps,

Register: 0x0000 (BMCR)
0x3100 (Speed Select=100Mbps, Auto-Negotiation Enable, Full-Duplex) à  Link OK
0x2100 (Speed Select=100Mbps, Auto-Negotiation Disable, Full-Duplex) à Link Fail

The customer assumed that they would link at 100Mbps since auto-negotiation is OFF, but actually the link failed. They asked us whether this behavior is correct for an IC. Is this correct behavior?

Thank you,
T.Imai

  • Hi Imai,

    Register: 0x0000 (BMCR)
    0x3100 (Speed Select=100Mbps, Auto-Negotiation Enable, Full-Duplex) à  Link OK
    0x2100 (Speed Select=100Mbps, Auto-Negotiation Disable, Full-Duplex) à Link Fail

    Please confirm that this is settings for DP83822. DP83TC811 does not support configuring speed select or auto-negotiation. 

    The customer assumed that they would link at 100Mbps since auto-negotiation is OFF, but actually the link failed. They asked us whether this behavior is correct for an IC. Is this correct behavior?

    Why is customer turning off auto-negotiation on DP83822? Auto-negotiation is useful for converging on link capabilities with link partner. Without auto-negotiation, manual settings need to be configured in the right order for link-up. 

    If customer must use auto-negotiation, try disabling auto-MDI/x with register 0x0019[15] = 0

    Lastly, why is customer using DP83TC811? DP83TC812 is a newer device with similar functionality as DP83TC811.

    Best,

    Charles

     

  • Hi Charles-san,

    Thank you for your reply.

    > Register: 0x0000 (BMCR)
    > 0x3100 (Speed Select=100Mbps, Auto-Negotiation Enable, Full-Duplex) à  Link OK
    > 0x2100 (Speed Select=100Mbps, Auto-Negotiation Disable, Full-Duplex) à Link Fail

    The above is the register of DP83TC811.  This setting is described in the data sheet 7.6.2 as follows.

    I have not heard why the customer is turning off auto-negotiation on the DP83822. I'll check it.

    I think register 0x0019 [15] =0 is a DP83822 register. 

    1) Please let me confirm, should we set register 0x0019 [15] =1 of DP83822 when using Auto-Negotiation?

    2) Does TI recommend using auto-negotiation because it helps converge link functions with link partners?

    3) This is the first question. The customer assumes that both the DT83TC811 and DP83822 should be linked at 100M because the auto-negotiation of the bothe ICs are OFF. However they saw the two ICs can't be linked. Is the phenomenon that the two ICs can't be linked is right behavior in this case?

    Regarding why the customer is considering the DT83TC811, the customer plans to develop a system that can connect a regular LAN and an in-car LAN, and use the system to develop and debug in-car networks. And also because it is also used in the DP83TC811EVM. They are planning to develop something exactly like DP83TC811EVM.

    I would appreciate it if you reply to the above three questions.

    Thanks & Regards,
    T.Imai

  • Hi Imai-San,

    Let me check in with my team. I'll have a response by end of day on Thursday.

    Best,

    Charles

  • Hi Charles-san,

    Thank you. I am looking forwad to hearing from you on Thursday, in Japan on Friday.

    Best Regards,

    T.Imai

  • Hi Imai-San,

    Lets take a step back. DP83TC811EVM should work out of the box. No registers should be written on the PHYs. 

    1. Please ensure one DP83TC811 is set to slave mode, and the other DP83TC811 is set to master mode. 

    2. Please ensure both DP83TC811 are set to autonomous mode. 

    3. Please read out register 0x0001 on DP83822 and DP83TC811 when both DP83TC811EVMs are connected. 

    Best,

    Charles

  • Hi Charles-san,

    Thank you for your quick response. I informed your reply to the customer and asked them to answer to your three questions.

    Do you need information about your three new questions to answer the customer question? If not, please reply as soon as possible.

    Thanks & Regards,

    T.Imai

  • Hi Imai-san,

    1. Please ensure one DP83TC811 is set to slave mode, and the other DP83TC811 is set to master mode. 

    2. Please ensure both DP83TC811 are set to autonomous mode. 

    3. Please read out register 0x0001 on DP83822 and DP83TC811 when both DP83TC811EVMs are connected. 

    Point 1 and 2 are not questions. They are actions customer should take to solve EVM no link-up issue.

    Customer should answer question and tell you what data is in register 0x0001.

    Best,

    Charles

  • Hi Charles-san,

    Thank you for the explanation. I received the following reply from the customer.

    1)Yes, one DP83TC811 is set to slave mode, and the other DP83TC811 is set to master mode. 

    2)The link fails between PC and the DP83TC811.
         When the auto-negotiation of the board is ON, the link succeed whether the auto-negotiation of the NIC of the PC is ON or OFF.
         When the auto-negotiation of the board is OFF, the link fails whether the auto-negotiation of the NIC of the PC is ON or OFF.

    3)The value of address 0x0001 of the DP83TC811 is,  when link succseeded : 0x786D,   when Link failed  : 0x7849.

        The value of address 0x0001 of the DP83822 is, when link succeeded : 0x0061,  when link failed : 0x0061

    The customer is evaluating the system with the following configuration.

    PC ― DP83TC811EVM ― DP83TC811EVM ― PC,  with using USB-2-MDIO.

    If the customer tries to communicate at 100Mbps from a PC, the link fails. Could you please tell us if this is normal behavior?

    Best Regards,

    T.Imai

  • Hi Imai-san,

    3)The value of address 0x0001 of the DP83TC811 is,  when link succseeded : 0x786D,   when Link failed  : 0x7849.

        The value of address 0x0001 of the DP83822 is, when link succeeded : 0x0061,  when link failed : 0x0061

    I believe you have the devices flipped. Read 0x0061 should correspond with DP83TC811. Am I correct in this assumption? 


    I will give advice based on this assumption : 

    The value of address 0x0001 of the DP83822 is,  when link succeeded : 0x786D,   when Link failed  : 0x7849.

    The value of address 0x0001 of the DP83TC811 is, when link succeeded : 0x0061,  when link failed : 0x0061


    From above register, DP83TC811 never links up. For correct link-up, we expect DP83TC811 device register 0x0001 = 0x0065.

    Please have customer check if this is the configuration of the EVMs: 

    Best,

    Charles

  • Hi Charles-san,

    This is just an update. The customer replied that the values of DP83TC811 and DP83822 were reversed.

    Therefore, the link failure occurs on the DP83822 side, and it occurs when the DP83822 link is set to auto-negotiation OFF.

    The 0x0001 register of the DP83TC811 is the value of 0x0065 when link is ok.

    I am checking if the customer has any additional questions. I will let you know the result.

    Thanks & Regards,
    T.Imai

  • Hi Imai-san,

    Thanks for the update. I'll keep this thread open for now. 

    Best,

    Charles

  • Hi Charles-san,

    I received new inquiry from the customer about link between DP83822 abd their PC.

    The customer informed me that the link between the PC and the DP83822 on the DP83TC811EVM is possible when the auto-nego of the DP83822 is set to OFF (bit 12 of the 0x0000 register =1), but not when it is set to 0. Is this behavior expected?

    Thanks &Regards,
    T.Imai

  • Hi Charles-san,

    Could you answer the customer's question above?
    Thanks & Regards,
    T.Imai