Part Number: DS90LV001
Other Parts Discussed in Thread: SN65LVP19
Hi team,
I would like to check with you LVDS buffer. Do we have device to support below conditions?
impedance supports 85ohm
VOD swing to support 800mV
Thanks,
Oliver
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Where do these specific values come from?
That would require a 9.4 mA driver. LVDS is designed for 350 mV over 100 Ω (3.5 mA); M-LVDS, for 570 mV over 50 Ω (11.3 mA), so an M-LVDS buffer might work with this. But M-LVDS signals are bidirectional, so there are no simple buffers.
Hi Oliver,
If you want an 800mV VOD, that would no longer be LVDS. That sounds like you are using LVPECL instead. A buffer like SN65LVP19 could be used here. However, LVPECL requires both lines to be terminated to Vcc -2 with 50Ohm resistors, bringing your total differential load to 100Ohms (see below). If you lower this to 85Ohms, you will see a lower VOD swing.

Regards,
Matt