Other Parts Discussed in Thread: DS92LV0422, DS92LV2421, DS25BR100, DS25BR110
Hello,
We're using the DS92LV2421 serializer, DS25BR100 repeater buffer, DS25BR110 receive buffer, and DS92LV0422 deserializer. The components are located on three different boards: the 2421 is located on a graphical processor board, the BR100 is located on a backplane board (the processor board plugs into the backplane board with 2mm hard metric connector set), the BR110 and 0422 are located on a display interface board, and the serial data stream between the BR100 and BR110 pass through a 3 foot custom cable with 100 Ohm STP. The serial data stream is AC-coupled with 0.1uf coupling caps, per the data sheets for the serializer and deserializer. All the power pins of the serializer and the deserializer are filtered with ferrite beads. Our pixel clock is at 66.4MHz. The 24-bit RGB data, control signals and clock being presented to the 2421 are not violating the 2421's input requirements. The issue we're having is intermittent flickering of the display. The flickering comes for a short period of time and then dissipates and the display operates just fine for about an hours and then the flickering comes back for a couple of minutes and then goes away again. We can count about 300 loss of lock during the flickering time. I can provide a schematic of the link if desired. I have tried replacing the coupling caps with 0.01uf and that helped, but didn't solve the problem. Please help.
Thanks,
Walid