This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB7320: TUSB7320 questions

Part Number: TUSB7320

Hi,
My customer has some questions of TUSB7320.  Could you please answer them?

*1
When they do not use the following pins, which is treatment, pull-up, pull-down or floating?
USB_SSRXP_DN2,  USB_SSRXN_DN2,  USB_DM_DN2  USB_DP_DN2

*2.
Which frequency (24MHz or 48MHz) of OSC/Crystal does TUSB7320 use as default?
Also, could you please let us know the pin/register setting related with clock frequency?

*3.
Could you please let us know the sequence limitation of both GRST# and PERST#?
My customer wants the following.  Could you please let us know any issues?
  De-Assert (Low->High) : GRST# -> PRST#
  Assert (High->Low) :  PRST# -> GRST#

*4.
Which type of PWRON# configuration, "Open Drain" or "Push-pull" pin?
I seem Pull-pull pin, but please advise us.

*5.
What is purpose of SMI pin?

*6.
What is purpose of JTAG pins?

Thanks and best regards,
M.Hattori.

  • *1
    When they do not use the following pins, which is treatment, pull-up, pull-down or floating?
    USB_SSRXP_DN2,  USB_SSRXN_DN2,  USB_DM_DN2  USB_DP_DN2

    these pins can be floating.

    hich frequency (24MHz or 48MHz) of OSC/Crystal does TUSB7320 use as default?
    Also, could you please let us know the pin/register setting related with clock frequency?

    48Mhz crystal should be used.

    Which type of PWRON# configuration, "Open Drain" or "Push-pull" pin?
    I seem Pull-pull pin, but please advise us.

    PWRON# is push pull pin.

    What is purpose of SMI pin?

    SMI  used  by BIOS software to enable System Management Interrupts

    *6.
    What is purpose of JTAG pins?

    JTAG pins are J-Tag interface for ATE testing for boundary scan.

    I will give more details about GRST later.

    Best

    Brian

  • Brian-san,

    Thank you for your support.  I have the additonal questions.  Could you please answer the following?

    *3
    Could you please let us know the sequence limitation of both GRST# and PERST#?
    My customer wants the following. Could you please let us know any issues?
        De-Assert (Low->High) : GRST# -> PRST#
        Assert (High->Low) : PRST# -> GRST#

    *7
    We can see the power-down sequence on the datasheet 7.3.1.2.

    >7.3.1.2 Power-Down Sequence
    >1. Assert PERST# to the device.
    >2. Remove the reference clock.
    >3. Remove the 3.3-V and 1.1-V voltages

    Is it OK for TPS7320 to do PETST#, reference clock and power on the same timing? If you have any time requirement on each lines, please advise us. (For example, PERST# assert timing is required PCIE_REFCLK, but VDDA/VDD33 and VDD11 power-down is same time. etc.)

    *8
    Datasheet writes PD/PU status on each pins. Could you please let us know "internal PD register value" and "internal PU register value" on each pins?

    Thanks and best regards,
    M.Hattori.

  • Could you please let us know the sequence limitation of both GRST# and PERST#?
    My customer wants the following. Could you please let us know any issues?
        De-Assert (Low->High) : GRST# -> PRST#
        Assert (High->Low) : PRST# -> GRST#

    GRST# should be low at  least 3 ms after both 3.3v and 1.1v are stable.

    PERST should be low at least 100 ms after both 3.3v and 1.1v are stable.

    PERST should be low at least 100 us after both PCI_CLK is stable

    Datasheet writes PD/PU status on each pins. Could you please let us know "internal PD register value" and "internal PU register value" on each pins?

    around 22k for internal PU/PD resistor

    Is it OK for TPS7320 to do PETST#, reference clock and power on the same timing? If you have any time requirement on each lines, please advise us. (For example, PERST# assert timing is required PCIE_REFCLK, but VDDA/VDD33 and VDD11 power-down is same time. etc.)

    You do need to assert PERST first but no timing requirement.

    Best

    Brian

  • Brian-san,

    Thank you for your support.  But I have one addional question.  Could you please let us know the status of each pins on GRST# condition?

    GRST# : Low GRST# : High

    Status of JTAG_TCL/TDI/TDO/TMS

    ?? ??

    Status of GPIO0-3

    INPUT (High-Z)?? Input (High-Z)??

    Thanks and best regards,
    M.Hattori.

  • Hi M.Hattori.:

         Do you use J-tag or GPIO pins? if not , just leave it unconnected.

    Best

    Brian

  • Hi M.Hattori.:

         If you don't use Jtage, just pulldown on Jtag_RST pin and leave all other Jtag pins floating.

       If you use J-tage, You need to pullup all jtag pins ( except Jtag-TDO)

    Best

    Brian

  •  If you don't use GPIO pins, just  leave all other GPIO pins floating.

    If you use GPIO pins, need to pullup GPIO pin used.

    the status when GRSTz low is no matters.

    Best

    Brian