This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN11623-Q1: Use TCAN11623 only as an LDO

Part Number: TCAN11623-Q1

Hi, for a special hardware application we consider using only the 3,3V LDO part. CAN is not connected, and no input signal on the local wakup. nSLP is connected to Vldo. Is there any risk that it can accidentally enter sleep mode caused by electric noise, or a low voltage dip?