This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB949-Q1: I2C communication

Part Number: DS90UB949-Q1

We are currently evaluating the DS90UB949 serializer in our development setup with the DS90UH948 deserializer and an external EDID EEPROM. We have observed the following behavior:

  1. When we perform a normal power-up or toggle the PDB pin cleanly, the HPD pin does not go high immediately, even though the I²C interface is accessible.
  2. If we short the PDB capacitor to reset the serializer, the HPD pin goes high immediately, but the I²C bus becomes unresponsive and all register reads fail.
  3. This issue occurs only when the 948 deserializer is connected to the 949 serializer.

Our questions:

  • What is the recommended method to safely assert HPD after a reset without causing I²C timeouts?
  • Is there a software-based reset sequence we can use via I²C to initialize the 949 while ensuring HPD goes high?
  • Could you provide guidance on timing requirements between PDB release, HPD assertion, and I²C readiness for a 949 → 948 link with external EDID?