Part Number: SN65LVP20
We need to connect to old obsolete TLK1521 Serdes input , because TLK1521 is obsolete we are using a SN65LVP20 Serdes LVPECL output instead.
Can you help us understand what are the recommendation for such connection :
- What is the recommended termination on the SN65LVP20 side ? we understand that we need to put pull down to GND on TXP & TXN , is it correct ? if yes what shell be the pull down value ?
- I understand that there is internal termination in the TLK1521 :
Do we need to add additional termination on the receiver side ?
- The TLK1521 is 2.5V supply operation , What shell be the supply voltage for the SN65LVP20 : 2.5V or 3.3V ?
- Do you have a IBIS model for SN65LVP20 for 2.5V operating , the current IBIS model in the website is for 3.3V ?
- Shell we put series capacitor on the P & N signal between the 2 ICs ? if yes 100nF value o.k. ?
- Please add any other info if I missed something .