Part Number: TUSB8043A
Hi All,
I have some questions about the TUSB8043AI.
(1) I have a question about writing to the EEPROM via a USB hub.
As stated on page 17, section 8.3.3 of the datasheet,
Is my understanding correct that:
- Programmable via the USB hub's Upstream port
- Programmable via the USB hub's Downstream port
Is my understanding correct?
(2) I have a question about operation in I2C mode.
I have a question about reading the EEPROM when powering on in I2C mode.
As stated on page 22, section 8.4.2 of the datasheet, if the EEPROM has not been written to, the data at address 00h is not 55h, so is it correct to assume that it will start with the default settings?
Also, is it correct to assume that the settings set by hardware strapping are valid in that case?
Best Regards,
Ishiwata