This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ESD451: Protection for HDMI

Part Number: ESD451
Other Parts Discussed in Thread: TDP158

Hi team,

I'm looking for HDMI protection device with clamping voltage at 8A Ipp IO to GND to be 4.5V or less.

Because ESD protection issue with TDP158.

Current ESD protection device is DF2B6M4BSL and it seems to be PUSB3FR4 for low clampling voltage.

TDP158: OE pin - Interface forum - Interface - TI E2E support forums

Do you have any ESD device such as PUSB3FR4?

Best Regards,

ttd