This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD2452V-EP: DE and RE# Tied Together?

Part Number: THVD2452V-EP

Hi Team, 

 

I am investigating the THVD2452-EP and whether or not this device can be configured as a half-duplex. However, one question that came up is whether the signal pins DE & RE# be tied together so a single source can be used? In addition, I'm not sure whether the logic levels internal to the part will dictate whether to enable DE or RE#.

 

Is the team able to provide any guidance here on how to achieve this with the THVD2452-SP? 

 

Thank you,

Filipe Rubinstein