This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX3223: Transmitter section failure of MAX3223IPW

Part Number: MAX3223

Hi in one application for MAX3223IPW , the force on is connected with invalid bar pin with zero ohm resistor. By mistake the force on is also connected with ground using zero ohm resistor. Initially the ic was working fine, now the tranmit section on RS 232 is sending garbage while the recive section of rs232 of ic is working fine. Can you tell due the invalid bar pin is connected to ground has done the damage to the IC?

 

Thank you.