This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS560DF810EVM: Reference clock output

Part Number: DS560DF810EVM
Other Parts Discussed in Thread: DS560DF810

Hello, I am SJ from Opticore.

 

We were using the DS560DF810EVM to create 25G PAM4 signal with two 25G NRZ signal.

 

But we realized there were no clock_output to trigger the Osciloscope (DCA).

It seems J3 is giving out the cal_clock of the J100, which is cal_clk_in which is 25G NRZ.

 

How do we get a 25G PAM4 clock trigger output? (ex- Change the settings in the board)

 

Thank you.

 

Regards,

SJ Ham

  • Hi SJ,

    Depending on what scopes you have available, scope may have CDR lock capability.  This could reduce the need for clock trigger output.  For example, DCA-X has this capability.

    The DS560DF810 does not have a recovered clock output.  The cal_clock is in a different clock domain than the data.

    As an alternative, can you use a trigger from your 25G NRZ pattern generator?

    Thanks,

    Drew