This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS110DF1610: What is the E suffix meaning in the ordering code

Part Number: DS110DF1610

Hi,

I would like to check what is the actual diffrence between the following 2 part numbers (E and without E).

Are they both eactly the same compoenent 1:1 ?

DS110DF1610FB/NOPB

DS110DF1610FBE/NOPB

 

Thank you.

Ido

  • Hi Ido-san,

    DS110DF1610FBE/NOPB and DS110DF1610FB/NOPB are exactly the same component. 

    The only difference between the two orderable part numbers is the Box Quantity (JIT MOQ):

    • DS110DF1610FB/NOPB → Box Qty = 630 (5 trays of 126)
    • DS110DF1610FBE/NO → Box Qty = 126 (1 tray of 126)

    The suffix "E" in DS110DF1610FBE denotes an evaluation/smaller reel or tray quantity variant, which aligns with the lower box quantity (1 tray vs. 5 trays).

    Best,

    Charles