This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC1T45: SN74AVC1T45DCKR SPEC question

Part Number: SN74AVC1T45

Hi team,

The datasheet for the SN74AVC1T45DCKR does not provide the maximum propagation delays (tPLH, tPHL, A to B, and B to A) when VCCA is supplied with 3.3V and VCCB with 1.2V, only typical values, while maximum values are specified for other power supply conditions.
Please help check the maximum delay values for tPLH, tPHL, A to B, and B to A across the full temperature range (-40~85°C) when VCCA supplies 3.3V and VCCB supplies 1.2V. Thank you.