This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS93A: Expected Problems with Decoupling Capacitor Changes to SN65LVDS93A

Part Number: SN65LVDS93A

Hi,Ikram,

When the decoupling capacitor is attached to SN65LVDS93A with 0.47uF instead of 0.1uF+0.01uF, the intermittent behavior abnormality occurs, and I wonder what the approximate cause is.

When I asked ChatGPT (0.1uF -> 0.47uF) the possibility of deteriorating the performance of high frequency noise cancellation, the possibility of increasing PLL jitter in VDDPLL, the possibility of increasing startup time, the slow rise time of VDD
I received a reply that there may be problems such as delay in reaching POR threshold and possible delay in initial LVDS output enable.
Please give me your opinion.
Thank you.