Part Number: TCA9539-Q1
Hello, I would like to inquire about the GPIO processing speed of the TCA9539-Q1 I²C expander IC.
In this application, the GPIOs will be configured as inputs, and we plan to use 15 pins (excluding one pin) on the TCA9539-Q1.
Each signal is expected to arrive approximately every 10–20 ms and does not have a periodic cycle like PWM.
Under this structure, even if all GPIO signals change simultaneously, we would like to ask whether the TCA9539-Q1 can process all inputs and output them via I²C without issue, and request your opinion on the approximate processing time.
Thank you.