Part Number: TSWDC155EVM
Other Parts Discussed in Thread: ADC3669, , ADC3669EVM
Hello,
I was able to evaluate an ADC3669EVM with the TSWDC155EVM and the ADC3669 GUI. Now I am tasked with writing a custom design for the Artix-7 FPGA on the capture board so we can capture longer sequences upon detection of a trigger signal instead of launching the capture solely via GUI.
It would be of great help if a .xdc constraints file specifying the interfaces between the FPGA and other system components was available. Unfortunately I did not find such file on the official product page, but before I start to manually extract the information from the schematics I wanted to make sure that an .xdc file is indeed not provided.
Regards,
Lennart