Part Number: TPD4E02B04-Q1
Dear Sir or Madam,
I am currently evaluating the TPD4E02B04-Q1 for use in an Ethernet application (1000BASE-T PHY-side MDI), and I would like to better understand its internal behavior and suitability.
From a system perspective, I understand that the TPD4E02B04-Q1 is a multi-channel ESD protection device with very low capacitance, intended for high-speed interfaces.
However, I have a question regarding its internal clamping topology and behavior under ESD stress.
My current understanding is that the device uses an internal rail-referenced clamping structure (even though there is no explicit VCC pin), and that during an ESD event, the internal nodes may not be perfectly symmetric for positive and negative stress conditions.
Based on this, I would like to confirm the following points:
1. During an ESD event, does the current path differ between positive and negative strikes due to the internal clamp topology?
In other words, are the conduction paths inherently asymmetric?
2. If there is such asymmetry, is it possible that this could introduce common-mode disturbances on differential lines (for example, Ethernet MDI pairs)?
3. Given this behavior, could you explain why TPD4E02B04-Q1 is listed as applicable to Ethernet interfaces (10/100/1000 Mbps) in the datasheet?
Specifically, is this intended usage more suitable for:
- cable-side protection or phy-side protection, or
- cases where a DC reference is well-defined?
4. For transformer-coupled, AC-coupled differential interfaces such as Ethernet PHY-side MDI,
are there any specific conditions or recommended usage guidelines when applying this device?
I would like to better understand the design considerations behind its Ethernet application usage.
Thank you very much for your support.
Best regards,
Makoto Kono