This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB7340: Camera output issue

Part Number: TUSB7340

Hi team,

We are using TUSB7340 in Robotics application.

  • Hardware Configuration: SoC -> PCIe -> TI USB host -> 3 USB cameras.
  • Upon system startup, a stress test involving continuous video streaming from the three USB cameras was conducted. After approximately 18 hours (the exact duration is unconfirmed, but the issue appears to manifest only after prolonged stress testing), the camera connected to port USB 2-2 stopped outputting frames. Please refer to the logs for kernel error messages. Details of the various test scenarios are attached. Currently, the USB 2-2 port on the TI USB host is suspected to be the cause.
  • Test details are as follows:
    • Test 1: Three cameras streamed simultaneously; after over two days of stress testing, the camera on port USB 2-2 reported an error (Kernel error: `WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state`) and the FPS dropped to 0.
      Analysis: The root cause was unclear; the stress test was repeated.
    • Test 2: Three cameras streamed simultaneously; after over two days of stress testing, the camera on port USB 2-2 reported an error (Kernel error: `WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state`) and the FPS dropped to 0.
      Analysis: The "left camera" failed with 0 FPS in both instances, raising suspicions about the camera itself. Test 3 was conducted.
    • Test 3: The cameras connected to USB 2-2 and USB 2-3 were swapped, along with their USB cables. After approximately two days of stress testing, the camera on port USB 2-2 again reported an error (Kernel error: `WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state`) and the FPS dropped to 0.
      Analysis: Camera and USB cable issues were ruled out. Suspicion shifted to the USB 2-2 port or the PCB circuitry. Since the issue only appears after a long duration, it may be temperature-related.
    • Test 4: The "MA" board was replaced with an "MB" board (mainboard replacement), while all other conditions remained unchanged. After 14 hours of stress testing, the camera on port USB 2-2 again reported an error (Kernel error: `WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state`) and the FPS dropped to 0.
      Relevant kernel log: (kernelMB_6.9.log)       

        4,49695,51211548032,-;xhci_hcd 0000:02:00.0: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.

         SUBSYSTEM=pci

         DEVICE=+pci:0000:02:00.0

        4,49696,51211549136,-;xhci_hcd 0000:02:00.0: WARN Set TR Deq Ptr cmd failed due to incorrect slot or ep state.

         SUBSYSTEM=pci

         DEVICE=+pci:0000:02:00.0

        6,49697,51211751735,-;usb 2-2: reset SuperSpeed USB device number 3 using xhci_hcd

         SUBSYSTEM=usb

         DEVICE=c189:130

        6,49698,51211781284,-;uvcvideo 2-2:1.1: Unknown video format 20343159-0000-0010-8000-00aa00389b71

         SUBSYSTEM=usb

         DEVICE=+usb:2-2:1.1

        6,49699,51211781296,-;usb 2-2: Found UVC 1.10 device Orbbec Gemini 215 (2bc5:0808)

         SUBSYSTEM=usb

         DEVICE=c189:130

        6,49700,51211785583,-;usb 2-2: Found UVC 1.10 device Orbbec Gemini 215 (2bc5:0808)

         SUBSYSTEM=usb

         DEVICE=c189:130

        6,49701,51211792801,-;usb 2-2: Found UVC 1.10 device Orbbec Gemini 215 (2bc5:0808)

         SUBSYSTEM=usb

         DEVICE=c189:130

 

Test 5: Stress testing the MB (Board 124) using the original three cameras. An issue occurred after approximately 50 hours of stress testing, specifically affecting the camera on usb2-2. (Relevant log: 124_issue/xhci_rootcause_20260608_152520)

 

Log:

  • Hi Gary:

     The "Set TR Deq Ptr cmd failed" warning indicates that USB host controller tried to clear or reset a data transfer  for a specific device, but the device or port state changed unexpectedly. It  was usually caused  by device disconnection, or the device was set into autosleep mode by Linux host.

    After issue happened, did customer check if the camera was still connected by lsusb command?

     from port driver below, all three ports have different drivers, was usbfs driver for full speed device and uvcvideo driver for camera?

    what speed for camera? high speed or full speed? in bulk data mode to Isochronous mode?

    since only port 2 has issue? any difference for layout between port 2 and port 1 and 3, did customer try port 1.3.4?

    Best

    Brian