Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDP20MB421: TDP20MB421 gains values

Part Number: TDP20MB421

I am using the TDP20MB421 as a DisplayPort mux and equalizer.

I am working with two DisplayPort input cables: one is 3 meters long and the other is 5 meters long. What gain setting should I use for each cable?

Is there a table or guideline that specifies which gain setting should be used for different cable lengths?

I am referring to the GAIN pin (Pin 1) and the EQ0 and EQ1 pins (Pins 40 and 20).

  • Hi,

    Do you know the insertion loss of the 3m and the 5m cable at the required Nyquist frequency? For Gain pin, you can leave it open. But for EQ0 and EQ1, we need to know the total insertion loss of the pre-channel in order to properly configure EQ0 and EQ1.

    Thanks

    David

  • what is the standard losses in DIsplayPort: 
    1. FHD, 60HZ, 3meter or 5meter standard cable?
    2. 4K, 60HZ, 3meter or 5meter standard cable?

  • Hi,

    The DisplayPort spec does not provide a specific insertion loss for specific resolution. It defines the Insertion Loss and Insertion Loss Fit curves for the cable assembly at HBR3, HBR2, HBR, and RBR data rate. 

    FHD@60HZ will be RBR or 1.64Gbps. 

    4k@60Hz will be HBR2 or 5.4Gbps. 

    Please check with the cable vendor on what the 3m and 5m cable loss will be at Nyquist frequency of 820MHz (for RBR) and 2.7GHz (for HBR).

    Thanks

    David