This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

pre-emphasis on a DS90C387-DS90CF388 link.



We use a DS90C387-DS90CF388 link for many years to make a display link with a cable of 15m. On the design we set the pre-emphasis level according to our 15m cable.

Now we want to use the same board-pair with different shorter cables (1m, 5m, 10m). With a shorter cable you can expect overshoot at the receiver side (too much pre-emphasis).

Is this allowed or will the receiver be overstressed?

Thanks, Stijn.

  • Greetings -

    Glad to hear you like the device and have been running 15 meters for years.  That is a good length and it sounds like you also have a good cable.

    You are correct, for the shorter cables, you ideally want to turn down the pre-emphasis level to obtain the optimual signal quality.  I am not too concerned with the over voltage effect to the RX input, it is pretty robust and allows for large VID and rail to rail levels.  I suspect at 1meter you might not need it enabled at all, and if you are happy at 15 meter use a setting for 1/3 and 2/3 for the 5 and 10 meters.  Ideally use a high bandwidth differential probe (eg TEK P6330) at the RX input to view the resulting signal quality and dial it in for the best eye and minimum overshoot.

    Please also make sure your shorter cables are of the same quality as your 15m one.  Usually pair-to-pair skew is the limitation on this typeof interface and skew should be minimized.

    Best Regards;

    John Goldie

    DPS APPS / SVA

  • Dear John,

    Thanks for the reply.

    To explain the situation more in detail:

    We would like to use the same board (with pre-emphasis resistor setting based on the 15m cable: 100Ohm, Vcc (100%) pre-emphasis) to drive the 1-15m cable-range. So when we use this board with a short cable (e.g. 1m) there will be for sure an overshoot at the receiver side. According to your replay this is allowed. Can you confirm this?    

    Thanks in advance,

    Kind Regards, Stijn.

  • Greetings -

    When you observe the waveform (check also single-endedly and differentially) - if the signal does not go below Ground or exceed VCC, then it is acceptable and not expected to do harm.  As noted over-equalization of a link will normally cause excess jitter and reduced sampling margin.  If however your settings, media, and resulting signal quality have acceptable margin for your application, then again you should be fine. 

    If the signals exceed the rails, you are generating extra noise sources and also turning on the ESD protection paths and this scenario is not recommended.

    I have seen some cables provide additional signals (for example two pins pulled to a combination of levels) that report back to the host what cable it is, then the proper settings can be set or switched in.  I understand your desire to use one set source board and this is not an option at this time.  Just sharing how others have self-configured for short, med and long cables to a single host board.

    John Goldie

    DPS APPS / SVA / www.ti.com