Other Parts Discussed in Thread: TUSB2036
Hello,
I've tried change the reset to ~3ms, utilizing a RC R=2,2K Ohm and a C=0.1uF and still entering in suspend mode.
I'm using a linux distribuition Angstrom. It can't enumerate the port, it says that the cable is bad.
It can't recognize the usb.
The module wich is processing the DM0 and DP0 is VAR-SOM-AM35.
The kernel linux is 2.6.32
Could you help me?
Best Regard,
Douglas Cogubum.