Part Number: SN65MLVD080
Hi TI Team,
I am using the SN65MLVD080 in a half-duplex M-LVDS application with an FPGA.
To reduce FPGA I/O count, I am evaluating whether the Driver Input (D) and Receiver Output (R) pins of each channel can be connected together and interfaced to a single FPGA bidirectional (tri-state) I/O.
I would like to understand whether directly connecting D and R together is a supported or recommended implementation.

My questions are:
1. Can D and R be directly shorted together and connected to a single FPGA bidirectional I/O?
2. If not, what prevents this approach? Is it due to output contention, internal device architecture, or another limitation?
3. Is there a TI-recommended circuit to achieve a single FPGA data I/O per channel using this transceiver?
4. If direct connection is not recommended, would adding external components (such as a resistor or logic gate) make this implementation acceptable?
Thank you.