This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9306DQER package parasitic uQFN package Ibis model

There are IBIS model on ti.com for the PCA9306  however, that ibis files do not include the package parasitics for the part I'm looking to evaluate. Can you provide the package parasitics for the uQFN package for part number PCA9306DQER and I can add that in the model file manually? Below is an example for what I'm looking for.

[Package] | typ min max R_pkg 5.000e-02 4.600e-02 5.500e-02 L_pkg 1.119e-09 1.025e-09 1.227e-09 C_pkg 3.520e-13 3.440e-13 3.630e-13

Thank you