Other Parts Discussed in Thread: PCA9306
Also, I have another question about the PCA9306 model. There is a model selector for the series pin mapping model PCA9306_IO_S. My design will use the 2.5V on the SCL1/SDA1 side and 3.3V on the SCL2/SDA2 side. Because I have two voltages, I'm not sure which of the options for PCA9306_IO_S to use in my simulations. What would you suggest?
Also which model would I use?
[Model Selector] PCA9306_IO_S
|
PCA9306_IO_25_S 2.5 volt Vcc
PCA9306_IO_50A_S 5 volt Vcc
PCA9306_IO_33_S 3.3 volt Vcc
PCA9306_IO_18_S 1.8 volt Vcc
PCA9306_IO_12A_S 1.2 volt Vcc