This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LV1224DB SN65LV1023ADB IBIS models



I am looking for IBIS models for SERDES parts: SN65LV1224DB SN65LV1023ADB I did not see them in the IBIS zip file on the website.

Thank you,

  • Frank,

    The IBIS model is attached.

    Regards,

    Atul Patel

    Texas Instruments

    sn65lvds1224_1023.ibs
  • I expected (was hoping for) values under the following line in the file, ideally with a comment labeled as being for the SSOP package.

    [Package]
    | variable typ min max
    R_pkg 0.0m 0.0m 0.0m
    L_pkg 0.0nH 0.0nH 0.0nH
    C_pkg 0.0pF 0.0pF 0.0pf

    Generally package values don't vary much part to part, so it is likely that TI has standard SSOP model parameters that I can paste in the file. These could be in a completely separate database from the IBIS files for the drivers.

    It is also possible, but unlikely, that the driver parameters are lumped with the package parameters and that is why the package was left as 0. If that is the case, please let me know and that will meet my needs.

    Thank you,