This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPLD1201-Q1: Temp Sensor Aggregator with Alert

Part Number: TPLD1201-Q1
Other Parts Discussed in Thread: TMP61, TPLD2001, TPLD1201

Hi Team,

I would like to see if it would be feasible to utilze the TPLD1201-Q1 as a temperature sensor aggregator with a single altert output.

In this usecase I would take 6xTMP61-Q1 devices and feed them into GPIOs of the TPLD device. If any of the TMP61 devices rise to a high enough voltage to indicate that it is >120 degrees I would like a output GPIO to go high as an alert function.

Let me know if you think this usecase is feasible with TPLD

Thanks,

David

  • Hi,

    Today is an American holiday, so responses will be delayed. I'll get back to you on Monday.

    Regards,

    Nikki

  • Hi David,

    Thanks for your patience. 

    This seems like a great use of TPLD. However, TPLD1201 only has two analog comparator , and it sounds like you need 6. Is that correct? In that case, I think you should be looking at TPLD2001 which has a total of 8 voltage comparators. If you give me more information, I can help you with the design.

    Regards,

    Nikki