This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVS5200: (IEC) Comparison Table

Part Number: TVS5200

Hi, Could you help provide a comparison table between ALPHA OMEGA AOZ8S516UDS and TI TVS5200?
Since TVS5200's package size (DFN1616, 6-pin) is bigger than AOZ8S516UDS (DFN1.6×1.0, 2-pin), I would like to know what superior features TI TVS5200 has that we can highlight in the comparison table to justify the size difference to the customer.
  • Hi Tim,

    Please see the comparison table below:

    Devices AOZ8S516UDS TVS5200
    Number of Channels 1 1
    Bi/Uni-Directional Unidirectional Unidirectional
    Working Voltage (Vrwm) 28V 52V
    Clamping Voltage (8/20us) 48V 58.9V
    Leakage Current (nA)  5nA 25nA
    Capacitance Typical (pF) 150pF 154pF
    IEC 61000-4-2 (Contact/Air) (kV) 30kV/30kV 15kV/15kV
    Surge Current 8/20 us 25A 25A
    Package Designator DFN1.6×1.0 DFN1616
    Package Size 1.6mm x 1.0mm 1.6mm × 1.6mm

    Why do you want to compare this device to the TVS5200? We have better crosses with the same Vrwm.

    Best,

    Bryan