This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP410: AC coupling and impedance

Part Number: TFP410

Dear Technical Support Team,

I have a question about the TFP410.

Q1

Generally, it seems that a 0.1 uF AC coupling capacitor is connected in series with the TMDS (TX) signal output line.
However, the TFP410 datasheet and other documentation do not mention adding a capacitor.
It states that the TX signal is routed directly from the device to the connector and that no external components are required.

Is it acceptable to omit the AC coupling capacitor?

 

Q2

When designing the PCB, should the differential impedance of the traces be 100 ohm?

Best Regards,

ttd

  • TTD

    Q1

    Generally, it seems that a 0.1 uF AC coupling capacitor is connected in series with the TMDS (TX) signal output line.
    However, the TFP410 datasheet and other documentation do not mention adding a capacitor.
    It states that the TX signal is routed directly from the device to the connector and that no external components are required.

    Is it acceptable to omit the AC coupling capacitor?

    TMDS is a DC-coupled interface, so AC coupling capacitors on the TMDS main link are not required.

    Q2

    When designing the PCB, should the differential impedance of the traces be 100 ohm?

    The differential impedance is 100ohm.

    Thanks

    David