This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS26LV31QML: Looking for the DS26LV31AQML Part

Part Number: DS26LV31QML
Other Parts Discussed in Thread: DS26LV32AQML

I am trying to source the DS26LV31AQML component

I was given this part number by engineering at NGC and am told that there are 7000 in stock at $50.00 each but I can not locate them on the site anywhere.

  • Hi Dan,

    I tried searching that device in our system but I don't see it showing up. I don't think we have a device that uses that 'A' suffix. 

    Is it possible that you have the incorrect device name?

    -Bobby

  • The corresponding line receiver is part number DS26LV32AQML.

    Also, the LVDS pair are DS90LV031AW-QML (Driver)  and DS90LV032AW-QML (Receiver)

    -Dan

  • I was able to locate the DS26LV32AQML in lit system. But the 31A version doesn't show up anywhere in either the lit database nor the automated testing database. I also searched for it in our PCN database incase it was EOL'd but no luck there either.

    If the part existed it would need to at least show up in the automated testing database unless it was hidden under an alias. 

    As weird as it seems this may have been a device that was developed as a standalone receiver without a driver pair (TI does this on occasion). 

    You may need to look at the non-A variant. 

    -Bobby

  • I do appreciate your efforts. It baffles me that I got not only the part number but also stock level (7000) and pricing ($50.00) from engineering at Northrop. Though they do say that it was quoted back on 9/4/2025

  • I'm wondering if maybe they got a quote (or an incorrect quote) for the ".A" version which is related to where the die was fab'd (for US vs. China tariff restrictions).

    -Bobby

  • This is likely incorrect; you need to reconfirm the components.

  • I have confirmed I was given the wrong part number