This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLIN1029A-Q1: Power up time(tPWR)

Part Number: TLIN1029A-Q1

Hello team,

I understand tPWR is time from power-up to RXD valid data output.

Does this power-up timing mean from at Vsup>0V or Vsup>4V(Vsup_min)?

Seeing from datasheet, there is no timing chart, can you share the timing chart?

Regards,

Youhei MIYAOKA

  • Hi Youhei,

    Although the data sheet does not explicitly define the starting threshold, based on the device operation:

    • The receiver is not guaranteed to operate below the under voltage threshold.
    • Hence, tPWR should be referenced from when VSUP has risen above the valid operating / under voltage threshold, rather than from 0 V.

    I.e., the timer should effectively begin once the device has sufficient supply voltage to exit under voltage and begin initialization, thanks.

    Best Regards,

    Michael.

  • Hello Michael,

    Understood. Thank you.

    Regards,

    Youhei