This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XIO2001: Need support of PCI to local bus device

Part Number: XIO2001

Dear Sir,

We have an industrial chassis that includes a PCI bus. We would like to translate the PCI bus signals to a local bus so that we can interface it with a memory device.

I was considering using the XIO2001IZAJ device, which is a PCI Express-to-PCI Bus Translation Bridge. I believe this device may be suitable for our application. However, I am not sure how to convert the PCI/PCIe signals into a local bus interface that can be used to control a memory device.

Is it possible to implement this functionality using an FPGA? i.e converting the PCIe signal (serial to paraller bus or converting to AXI bus). I would appreciate your suggestions on the best approach.

Additionally, please let me know if you have a PCI-to-local bus interface device that can perform this function directly.

Thank you for your assistance.