This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS30BA101: High Speed LVDS Data interface over a long CAT6 cable

Part Number: DS30BA101
Other Parts Discussed in Thread: DS15BA101, DS15EA101, DS30EA101,

Hi,

We want to use one of the 2 buffer pairs (either DS15BA101/ DS15EA101 or  DS30BA101/ DS30EA101) for high speed data transfer, 150Mbps, using LVDS signaling over a CAT6 cable for as long as 100m (and maybe longer).

The connection is between 2 processors, with LVDS Output/Input ports.

MCU_A ==>DS30BA101==>CAT6 cable 100 meters ==>DS30EA101==>MCU_B

 

Do you see any issue with this design?

Is one pair (DS15.. / DS30..) more suitable than the other? 

Any other option (parts) that we should consider?

Thank You,

Yerach