DP83867IR: Regarding the clock out of DP83867IR

Part Number: DP83867IR

Hi TI,

Here is my application, the SoC provides a 25MHz clock to the DP83867IR, and the DP83867IR outputs a clock to the SoC via CLK_OUT pin.
-The Ethernet throughput supports both 100 Mbps and 1 Gbps.

-A 24MHz crystal provides  the main clock source for the SoC.

My question is: Can I disconnect the CLK_OUT connection in my application?

2026-07-14_14h37_58.jpg

 

 

 

regards,

webber