This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DPHY440SS: De-Skew Function

Part Number: SN65DPHY440SS

Hi team,

what's the max skew that SN65DPHY440SS can compensate by using de-skew function?

Thanks!

Rayna

  • Rayna

    This is not the same de-skew function that is typically associated with a re-timer. The DPHY440 receives on the DA[3:0]P/N interface and provides a retimed version on the DB[3:0]P/N interface. The retimed version is centered within the DBCP/N clock. So there is no max skew number.

    Thanks

    David