This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83826AI: Issue with EtherCAT slave using DP83826A

Part Number: DP83826AI

I have developed a code for XMC4800 evaluation board which uses BCM5241XA1KMLG and it is working fine. Since it became absolute, I switched to DP83826A, and used the same working code, and added some additional code to configure DP83826A in accordance with the datasheet. However, no I am getting "INIT to PREOP failed! Error: read slave count. Commuication error 0x71f"
when I checked the slave state, I found it become INIT LNK_ERR LNK_ADD B for short time before it become INIT NO_COMM.
I can see the Activity LED changing the blinking rate with transition request and error, what possibly could be the issue here?