This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848I: questions about SNI mode 2

Part Number: DP83848I

Hello,

Related to the following E2E thread, my customer further questions as follows.

DP83848I: questions about SNI mode - Interface forum - Interface - TI E2E support forums

As described in the above E2E thread, DP83848I is powered up as SNI mode (RX_ DV/MII _MODE pin and TXD_ 3/SNI _MODE pin are pulled up). In this case, writing 1 to bit 14 (Loopback) of the Basic Mode Control Register (BMCR), the input signals into RXD_ pin are looped back to RX_0 pin?

Best regards,

K.Hirano