Part Number: DS160PR810
Other Parts Discussed in Thread: DS160PT801
SMBus/I2C Pull-Up Resistance Values When Not in Use
I have a question regarding the SMBus/I2C pull-up resistance values for the products listed below.
Part Number Pin Required Pull-Up Resistance
DS160PR810 GAIN0 / SDA 1 kohm to 5 kohm
RX_DET / SCL 1 kohm to 5 kohm
DS160PT801 SMBCLK 2 kohm to 5 kohm
SMBDAT 2 kohm to 5 kohm
EE_CLK 2 kohm to 5 kohm
EE_DAT 2 kohm to 5 kohm
The datasheet specifies that pull-up resistors should be connected as shown above.
Q1
Do these resistance values indicate that the total pull-up resistance during SMBus/I2C communication
just needs to fall within the specified range?
Q2
Do these pins have built-in pull-up resistors?
I would like to confirm whether a pull-up resistor of several tens of kohm should be added to the circuit when SMBus/I2C communication is not in use.
Note:
We are currently considering manually switching between SMBus and I2C communication using a jumper switch.