Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90CR286A: Input format check

Part Number: DS90CR286A

Hi TIer

My customer want to use DS90CR286A in LVDS to RGB in medical edoscope application.

Could you hlep check if DS90CR286A support SPWG mapping input? 

If we use SPWG any change we need to set in chip or schemtic?

Thank you very much.

  • Hi Tony,

    The device can support both VESA and JEIDA formats depending on how the schematic is done to ensure the output (RGB + HS/VS/DE) matches the input format.

    Yes, the device can support SPWG which is same as the VESA format. The VESA format has MSBs on RxIN3 so the device inputs should be connected as per datasheet table: "3. 8-Bit Color Mapping with MSBs on RxIN3±". So the output connections (RGB + HS/VS/DE) on the schematic will need to be based on the VESA format.

    App note for reference on OLDI to RGB mapping: https://www.ti.com/lit/an/snla014a/snla014a.pdf

    Best regards,
    Ikram