This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3DV642: Question about TS3DV642A0RUAR

Part Number: TS3DV642

Hello:

The application scenarios are as follows:
The mipi output of the main control SOC1 and the mipi output of the main control SOC2 are connected to the input of TI's TS3DV switch, and the mipi output of the switch is connected to the 5.48 screen. At present, the customer intends to use this switch to achieve time-sharing display of two DSI channels. May I ask if the TS3DV material is suitable for mipi switching between dual DSI screens?

Thanks!!!

  • Hello Jimmy,

    The TS3DV642 is a passive mux, so it can support any application as long as the signals it is passing through it are within its datasheet specifications. 
    I can confirm this device is suitable for mipi applications such as yours. 

    Thanks,

    Nir