This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX232E: MAX232EIDWR vs TRS232EIDWR

Part Number: MAX232E
Other Parts Discussed in Thread: TRS232E,

Dear Technical Support Team,

As a replacement for the SP232ECT-L/TR(WSOIC16), which of the pin-compatible MAX232EIDWR or TRS232EIDWR would you recommend in terms of long-term availability?

In past E2E articles, the TRS part numbers were recommended over the MAX part numbers, but the TRS232E package is almost end-of-life (EOL), whereas the MAX232E still appears to be available in packages such as TSSOP and PDIP.

MAX3232: Difference between MAX3232/E and TRS3232/E - Interface forum - Interface - TI E2E support forums

Best Regards,

ttd

  • Hi ttd,

    It shouldn't matter which one you choose now. We've finished our portfolio consolidation for the RS232 devices so both of them should be in the same bucket in terms of longevity now. 

    -Bobby