Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV8T541: Vin = VCC case

Part Number: SN74LV8T541

Hello, I want to interface 6x 3.3V signals with an FPGA. For this use case, it is possible that the FPGA I/O voltage could be 3.3V, 2.5V or 1.8V. For this reason, I want to tie VCC to the I/O voltage of the FPGA. I would like to confirm whether or not this level shifter could work in the case that the 3.3V input signals match VCC voltage. If not, are there any parts you could suggest for this application? Thank you.