This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1042H: NC pin confirmation

Part Number: TCAN1042H

Team,

Just one simple question. 

Customer using the TCAN1042H non V version. I know that is a NC pin at pin5. RD Just would like to double check with BU if pin5 is no connection?

 

 Layout guide: Terminal 5: For "V" variants of the family, bypass capacitors should be placed as close to the pin as possible (example C6 and C7). For device options without VIO I/O level shifting, this pin is not internally connected and can be left floating or tied to any existing net, for example a split pin connection