This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVS3300: Thermal Pad Connection

Part Number: TVS3300
Other Parts Discussed in Thread: LMR51450

Dear TI Support Engineer,

I want to connect two TVS3300 back-to-back to make a bidirectional TVS. My questions are: 

  1.  Can I leave the thermal pads floating?
  2. Can I not connect the two thermal pads together? See attachment for diagram
  3. If I also want to connect a ferrite bead to my DC line, do I place the ferrite bead before or after the TVS? See attachment for diagram

Please note that V_out in the diagram goes to the input of the buck converter LMR51450.

Thank you for your help.

Best regards,

Kua Cha

TVS3300.jpg